Other Parts Discussed in Thread: TPS628502 , TPS628302 , TPS628512 , TPS54418 , TPS54318 Tool/software: Hi,
I am looking for drop-in replacement of these two parts.
1. TPS54218RTET
2. TPS54218RTER
Any suggestions for drop-in replacement solutions…
Part Number: TPS54218 Hi support team,
The rush current on the output side at startup is approximately 1.28A. Is there any problem with the device? No current flowing backwards was observed at the input of TPS54218. I think it passes through the inside…
Part Number: TPS54218 Dear Team,
Can you please advise what are the differences between TPS54218 and TPS5418A ?
Same question has been asked on the following thread but without an answer.
https://e2e.ti.com/support/power-management-group/power-management…
Part Number: TPS54218
Hi support team, I have a question regarding TPS54218.
This is a phenomenon during shutdown, A jagged waveform like the one attached was observed on the input and output currents using an oscilloscope. A jagged waveform like…
Part Number: TPS54218 Other Parts Discussed in Thread: TPS54318 Dear,
customer is using tps54218, plan to change to tps54318, whether i use it directly ,no change any schematic;
Part Number: TPS54218 Hello,
I was looking at recommending this TPS54218 EVM for a customer to test the TPS54218. However, they would like the ability to change the switching frequency flexibly between the 300 and 2000 kHz range and output voltage and…
Part Number: TPS54218 Hi support team,
About the switching waveform of the PH pin. The Low level does not reach 0V, but is about 0.4V.
Please let me know the principle that it does not become 0V?
Regards, Dice-K
Part Number: TPS54218 About TPS54218, is there tolerate current rating for reverse current?
In the case of reverse current for the moment (by output side issue), it was occur about -1.8A.
I want to judge these current possibility to damage, or not…