Hi Joe,
Yes, the HFTF was added as an alternate site. The change in pad size is based on availability at the additional site. The change in pad size is only related to the HFTF site and does not affect the others.
Regards, Denislav
Part Number: TPS54240-Q1 TEXAS INSTRUMENTS - PCN : 20231220001.2 - Effective Date : 2024/06/20 - PCN Types : Fabrication site change / Qualification/Country of Origin/New Subcon (FAB)
About the "CS2305251: PPAP20231227-028858", Here I create…
Hi Frank,
Thank you for your reply.
I'll share the answer with the customer.
I hope the answer will be accepted by the customer.
If they have an additional question, I consult you again.
I appreciate your great help and cooperation.
Best regards, …
Part Number: TPS54240 Other Parts Discussed in Thread: STRIKE I have a question about PCN#20231222000.1.
<Question>
(1)Is the additional wafer processing plant CFAB located in Chengdu, China?
(2)Where is the new inspection factory CD-PR located…
Part Number: TPS54240 Other Parts Discussed in Thread: LMR51420 , LMR51430 Dears,
Customer feedback that the Continuous current diode during the end customer use process,pls help to check the schematic whether have any problem or not?
Thanks
Part Number: TPS54240 Other Parts Discussed in Thread: TPS54340B
Please let me confirm two points below about synchronizing to system clock.
①Is below schematic no problem?
Clock source is 3.3V CMOS output (Logic IC), it is not Hi-Z.
Clock source is…
Part Number: TPS54240 Other Parts Discussed in Thread: TPS54140 , Team,
Is the criterion of skipping mode between TPS54140 and TPS54240 the same? Or they're not the same?
Since system requirement in customer side, the original TPS54140 is changed to…
Hi Richard, My apologies for the delay. Your response really helped a lot. However, our customer can't change the compensation network circuit because the production is active and the components were already bought. Could you help us analyze whether their…
Part Number: TPS54240 Hello,
I am designing a power supply with a TPS54240QDGQRQ1 buck converter that reduce from 12V to 5V and load from 500mA to 2A.
Unfortunatelly this is old design and I have to keep some part fixed until I have option to change.…