Part Number: TPS54262-Q1 Other Parts Discussed in Thread: LMR38020-Q1 The datasheet of TPS54262QPWPRQ1 is not clear about the efficiency of the device when the input is 24V-27V. I do not want to assume what it is from the graph with 7V and 14V input.
In my customer setting, Vin range is 14V to 28.5V, output voltage is 13V.
At no load condition,
When Vin voltage drops down to 14V, output voltage drops down to 6V from 13V.
After that, even if BAT voltage recovers, output voltage doesn't recover up…
Other Parts Discussed in Thread: TPS54262-Q1 I am building a 12V to 8.5V switching power supply with the TPS54262-Q1, and I cannot find any information about how much current it can sink. I need to be able to sink and source up to 1A of current at 8.5V…
Other Parts Discussed in Thread: TPS54262-Q1 Hi,
The my customer is selecting compensation components for TPS54262.
And, he wants to know phase margin and gain margin.
How can he calculate phase margin and gain margin?
Thanks,
Kuramochi