Part Number: TPS54283 Hi I am looking for a mean time between failure or average lifespan rating or similar field for the TPS54283PWP buck converter. Any help would be appreciated.
Hi Jordan,
We have not seen an update from you for one month, so I assume the questions are answered and the issue is solved.
If you don't have any further questions, can you please close the thread by clicking on resolved. Clicking the Resolved Button…
Part Number: TPS54283 Other Parts Discussed in Thread: TPS54286 Hello together,
I'm currently working on Dual-Buck-Converter using TPS54x8x to convert 24V input-voltage to dual 5V outputvoltages. In the datasheet of the TPS54286, on page 42 is a design…
Part Number: TPS54283 I am using the TPS54283 dual non-synchronous converter ic for converting 24V DC input to 5V and 3.3 V output. Both designed for 2A current limit. there is a ringing noise present at both outputs. how to reduce that?
Part Number: TPS54283 Hello:
TPS54283 is a power supply solution for group 2 output. One group of TPS54283 works and the other group is in a suspended state. The output of TPS54283 is abnormal. As the attachment
Is TPS54283 working normally?
Best Re…
Part Number: TPS54283 Other Parts Discussed in Thread: TPS54160A Dear All,
I am looking for a DC/DC converter for Induction Motor EE Vin24V Vout=±15V to supply the dual supply ports of an OpAmp (+15V and -15V) 100mA each outputs.
Do we have anything…
Part Number: TPS54283
Hi, i implemented a dobule dc-dc buck regulator with TPS54283.
Output 1 is 3.8V 1A, output 2 is 12V 0.6A. Input volatge is 19.1V
Here is the schematic
The input voltage is always stable but:
This is what happen to output 1:
This…
Other Parts Discussed in Thread: TPS54283 Hi,
I am using TPS54283 DC-DC converter for my new application. I designed circuit for 5V,2A and 15V,0.7A outputs using Switchpro tool. I checked output current by increasing output load. But output voltage drops…
Part Number: TPS54286 Other Parts Discussed in Thread: TPS54283 , TPS54229 , TPS563201 , TPS563208 Customer is looking for an alternative solution to Diode's AP65111AWU-7, even non-p2p is acceptable. I check datasheets and seems some feature of TI's…
Part Number: DRV8806 Other Parts Discussed in Thread: TPS92518 , TPS54286 , , TPS54283 , TINA-TI I need a SPI-controlled buck-regulator with an output ranging from 12V to 24V with 0.5V step resolution. The input voltage is 28V and the max load is 1.5A. I…