Part Number: TPS5430 Tool/software: Hi TIer
Customer use our TPS5430DDAR like this schematic.
Output is 9V (250mA - 450mA)
The customer will get some abnormal SW waveform similar to DCM mode in a normal SW waveform with a switching frequency…
Part Number: TPS5430-EP Other Parts Discussed in Thread: TPS5430 Tool/software: Hi Sir,
Using TPS5430 can we achieve the following power stability
Power Stability : Unit- % ( RMS ,8 hrs, Range : 0.02 - 0.25)
Unit- % ( Peak to Peak ,8 hrs, Range…
Part Number: TPS5430 Hello,
Referencing slva257a and slvu243
If I configure a TPS5430 for negative output (between -3.3V and -15V), does that change the Vin range for the TPS5430.
Typically Vin is 5.5 to 36V (referenced to GND)
Does that change…
Part Number: TPS5430 Tool/software: Dear TI engineers,
I am developing a device which main supply has been posted on schematic below:
The input is standard 9-12V DC. I disconnected all the loads and placed a single resistor instead, as seen on the…
Part Number: TPS5430 Tool/software: Hi TIer
Could I ask a question, what do the closed-loop transfer functions and the individual factors of the TPS5430 relate to when I know these factors?
Could you explain how this formula came from?
Thank you…
Part Number: TPS5430-EP Hello,
I'm currently using TPS5430DDA. However, since it is difficult to obtain, I am considering using TPS5430-EP. Looking at the TPS5430-EP data sheet, the absolute maximum rating for PH is -1.2V. The TPS5430DDA has an absolute…
Part Number: TPS5430 Tool/software: Hello,
We are planning to use 24V to 5V, 1.5A(min), buck regulator in one of our designs.
I have one general query as below:
As this is new design, which TI buck regulator part is suitable to use which has good…
Part Number: TPS5430 Tool/software: 1. Can the subject part be configured to produce negative output voltages?
2. What is the true operating junction temperature of the subject part number? Can the part operate at 150C junction temperature?
Part Number: TPS5430 Hi,
Has this part been tested for electrical latchup? did it pass?
Was this part tested for any radiation effect?
Is the a BiCMOS?
Munir