Part Number: TPS54302 Hello,
I have used two TPS54302 chips in my design to generate two voltage sources 5V DC and 3V3 DC from a common source Vin ( range from 7V DC to 24V DC, 3A).
I have done several tests and see that I can obtain 5V DC and 3V3 DC…
Part Number: TPS54302 Hi Team,
My customer would like to know if there is Temp v.s FB voltage curve information?
Or,
when the temperate increase the Vfb will be increase or decrease?
Best regards,
Hardy
Part Number: TPS54302 Hi Expert,
Datasheet mention "The 49.9-Ω resistor, R1, is provided as a convenient location to break the control loop for stability testing" what situation we need to break the R1?
How to do the stability testing?…
Part Number: TPS54302 Hi team,
En pin requires Floating when buck IC PSpice simulation. However, this causes PSpice to be incorrectly reported as follows:
How does PSpice set up Floating? Thanks.
Best Regards,
Cherry
Part Number: TPS54302
Hi Team,
Customer would like to design TPS54302.
Would you please help review schematic/layer and provide your comments?
Here is the design material for TI internal access. (PW:ti2023)
https://txn.box.com/s/g1k5z2s51ctx60c4erg…
Part Number: TPS54302 Other Parts Discussed in Thread: TPS54308 Hello E2E Experts,
Good day.
When the TPS54308 was unavailable, we substituted the TPS54302 with no other cct modifications. The application is 24VDC input, +/-3.3VDC output at 1A.
Schematic…
Part Number: TPS54302 HI, Power mnagement forum team.
I want the webench/SPICE model of Inverting Buck-Boost (OUTPUT -5 V to -7 V) on the TPS 54302.
Would it be possible for you to prepare it?
regards
S.Ishikawa
Part Number: TPS54302 Hi,
I'm trying to use TPS54302DDCR for a 24V to 5V / 500mA step down supply with the following layout and components. I seem to get output voltage glitches when at around 100mA load where the voltage drops 1-2V for 100us and beyond…
Part Number: TPS54302 Hi Ti team,
When the 24V Adapter is inserted, the input inrush current will be as high as 22A, is there any risk of damage to the TPS54302. Please also help check the schematic below(Products use 6PCS TPS54302)