Part Number: TPS54308 Hi All,
I am using the TPS54308 for a 24V to 5V design.
All my calculations converge to the simulations and all is perfect except one thing. in the DS, it says that BOOT-SW voltage should be -0.3V to 7V. Looking at the DS and the…
Part Number: TPS54308 Other Parts Discussed in Thread: TPS54302 , LMR51430 Is there p2p compatible with TPS54308 (with PWM mode)? thanks.
Regards
Brian
Part Number: TPS54308 Other Parts Discussed in Thread: TPS54302 Hi,
I am using TPS54308DDCR in my design and found the power consumption is very high - 8.2mA with a 9V input and 3.3V output without any loads.
Do you have any ideas about what could go wrong…
Part Number: TPS54308 Hi,
I am trying to simulate an already working circuit using tps54308.
At first i was able to simulate, but the results were not reasonable... very strange behavior of the IC output... (0-320mV)
Now when i try to simulate .. it…
Part Number: TPS54308 Hi,
What's the difference of bode plot measurement btw flybuck and buck?
If I want to measure flybuck bode plot, should I add load to secondary winding or primary?
Thanks
BRs
Kian
Part Number: TPS54308 Hi,
I am trying to simulate an already working circuit using tps54308.
Transient simulation.
My first simulation parameters were 10ms simulation with 20ns step, and my output ripple was 6.78mVpp
I changed my simulation to run…
Part Number: TPS54308 Hello team,
My customer is consdering to use TPS54308 with Vin = 5.55V and Vout = 5V with 2A of max Iout.
Is it possible to operate in this condition? (It is about 90% duty from Vout/Vin)
The datasheet says it can operate in 100…
Part Number: TPS54302 Other Parts Discussed in Thread: TPS54308 Hello E2E Experts,
Good day.
When the TPS54308 was unavailable, we substituted the TPS54302 with no other cct modifications. The application is 24VDC input, +/-3.3VDC output at 1A.
Schematic…