Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS54308 Hi Dear,
Does TPS54308 support negative pressure output. The customer needs negative 10V output.
If yes, whether there is a design circuit for negative pressure output can be referred to..
Thanks
Part Number: TPS54308
Hi Experts,
Good day!
Regarding the datasheet for TPS54308, Figure 8-1 on page 13 says: 5-V, 3-A Reference Design, but in the figure it says VOUT=3.3V.
Could you confirm that the values in that reference design are for 3.3V output…
Part Number: TPS54308 Hi experts,
My customer want to use TPS54308 in the Flybuck circuit. But He met a error report when he simulated the circuit with PSpice for TI.
Below is the simulation circuit. The parameter is : Input voltage=15V, nos-isolated …
Part Number: TPS54308 About EN pin of TPS4308, datasheet is described "Float the EN pin to enable".
If there have any risks or careful points for EN pin left floating condition (more than external setting or connect Vin with resister), please…
Part Number: TPS54308 Recently if TPS54308 change the internal structure or manufacturing process, etc, please let me know these information.
Before and now , one customer is using TPS54308 on the same circuit, layout, and the other condition.
But recently…
Part Number: TPS54308 We use the TPS54308as part of a charging system for body-worn cameras for the security services and police but can't get delivery at sensible prices (the last price we paid was $30 !).
Is there any alternative or do we have to…
Part Number: TPS54308 Hi Sir,
I now use tps54308. If the feedback phase compensation capacitor C6 is used on the designed substrate, it is approximately more than 50pF, Does the protection circuit work when the power is turned on? Unable to output normally…
Part Number: TPS54308 Hi team,
Can TPS54308 work in 100% duty cycle mode?
Is there a chip recommendation? The application scenarios are as follows:
USB3.0 PD power supply, initial voltage 5V, about 800MA
After the system works. et the PD chip to make…
Part Number: TPS54308 Hi Team
Customer using TPS54308 for 12V to 3.3Vout convertion.
The EN PIN rising threshold is 4.5V with external resistor divider. There is a scenario when customer using external simulator for MCU software download, this simulator…