Part Number: TPS54326 Hi Sir,
I would like to know the input current of EN signal. I can’t find this data from the datasheet, could you please help to provide it ?
Thank you!
TPS54326
Part Number: TPS54326
Below you can see PS based on TPS54326RGT
VO=5.4V
What is min. VIN?
2)
. Pls. review the schematics below.
For Buck:
Vin: 4.5-18V.
Nominal 12V.
VO=3.3V, IO=3A.
Part Number: TPS54326 Team,
Could you please help with the below issue:
Two TPS54326 Devices are used to generate below voltages: P1V15_Aux ( 1.15V from 12V, @ 1A max.)
P1V2_Aux (1.2V from 12V, @ 0.7A max.) Observations:
•AT SW output pin, small pulses…
Part Number: TPS54326 Hi Team,
I have a customer using the TPS54326 and is having trouble:
"We got our new board but have troubles using the TPS54326 to generate +5.3A. I extracted our schematic and pasted below.
We isolated TPS54326 from input…
Part Number: TPS54326 Other Parts Discussed in Thread: TPS54335A , The threshold to leave skip mode is at much higher current level.
But at datasheet fig.10 shows that the level is around 50mA only.
Please directly see below scopeshots in different load…
Part Number: TPS54326 Hi guys,
My customer is evaluating the TPS54326, and they are using Vout = 5.3V. They had the following questions:
The Table 1 in switching regulator TPS54326 data sheet doesn’t specify the recommended component values for output…
Other Parts Discussed in Thread: TINA-TI Hi Team,
I understand that the maximum voltage of SS pin is 0.779V(it is maximum voltage of VFB).
Is my understanding correct?
And, I have one more question.
I simulated the following conditions using "TINA-TI…
Other Parts Discussed in Thread: TPS54326 Hi Team,
I have two questions about Figure 10.
[Q1]
Could you please let us know the input voltage?
I can’t find the input voltage condition of this data in datasheet.
[Q2]
I believe that the ranges of…
Other Parts Discussed in Thread: TPS54326 Team,
My customer found TPS54326 output discharge function is failed.
Please refer to below scopeshot.
Input is 12V, output 1.25V
While we pull down the enable signal, 1.25V output is drop.
But after 3 seconds…
Hi Could you tell me the recommended max Vout for Vin at 5V. I see the VREG5 need 6 to be in regulation. However what if i have 5V can i get to 3.3V Vout. I assume the VReg is a LDO so you have a minimum drop out voltage. Could you let me know if i con…