Part Number: TPS54328 Other Parts Discussed in Thread: TPS563211 , TPS563252 , TPS563203 , TPS563202 Hi Teams,
Do we have better replacement of the BD9D320EFJ?
BRs,
Marsh
Part Number: TPS54328 Hi Team,
May I ask if TPS54328 Have Maximum Css Limitation? My customer now set the Css=100nF in their system, and they would like to know if this will affect system performance, except for longer soft start time? Would you please…
Part Number: TPS54328TPS54328 is supposed to run with switching frequency close to 700kHz at steady state, but Webench shows in its report a frequency of 644kHz. For this particular application operating conditions are:
Vin = 5V
Vout = 1.5V
Iout = 3…
Part Number: TPS54328 Hello,
In the datasheet, there isn`t a drawing on the VSON 10 drawing. The page is blank. Can you please help on this issue?
https://www.ti.com/lit/ds/symlink/tps54328.pdf?ts=1624340712940&ref_url=https%253A%252F%252Fwww.ti.com…
Part Number: TPS54328 Hi team,
Customer would like to know what is the difference between TPS54328DRC and TPS54428DRC.
Except the current rating is 3A and 4A. Is there other different items needed to be aware of? They would like to do p2p replacement…
Part Number: TPS54328 Dear support member,
My customer used TPS54328.
I have a question.
Why the max output voltage range is regulated at 7V?
Best regard. Bob Lee.
Part Number: TPS54328 Hi team
My customer using the TPS54328 as the 16V to 4V function, the input is the four-cell Li-battery and the fully-charged battery voltage is about 16.4V, the load is a GPRS module in which the startup current can reach up to…
Other Parts Discussed in Thread: TPS54328 We have a question about TPS54328.
We want to check the relationship between output of VREG5 and temperature.
For example, variation of VREG5 by changing temperature.
Do you have the data or figure?
Best regards…
Part Number: TPS54328 Hi Team,
Please help me answer the follow question, thank you so much.
I am using TPS54328 to generate 5V to 3.3V. Current output 3.3V rise time is a problem. At present, a 3.3 nF capacitor is connected to the SS pin for soft start…
Other Parts Discussed in Thread: TPS54328 We have questions about input capacitor of TPS54328.
In datasheet p.13 8.2.2.3 Input Capacitor Selection,
TI recommends a ceramic capacitor over 10 µF for the decoupling capacitor.
Question 1.
Please tell…