Part Number: TPS54329E Other Parts Discussed in Thread: TPS54426 Hi team,
Customer cannot keep input capacitor as >10uF, which is the recommendation. The value is 6uF(effective input capacitance). Is it acceptable for the device?
They have same…
Part Number: TPS54329E Other Parts Discussed in Thread: TPS54339E , TPS54329 , TPS54229E , TPS563211 , TPS563200 , TPS563212 , TPS563231 , TPS563202 Hi Team,
Customer wants to use TPS54329EDDAR to replace TPS54329DDAR because device shortage directly…
Other Parts Discussed in Thread: TPS54329E Dear all
I use TPS54329E to 6V→5V,3A application.
According to the datasheet , when Io=3A, output drop voltage <50mV, which is shown on the page 1.
But the actual data I tested is as below:
when INPUT…
Not sure where to post this, but...
I've done a webench desigh using TPS54329E 6.0-16.0Vin, 5.0Vout 0.7A.
Webench lists 22uF ceramics for Cin & Cout.
Do these values take into account dc-bias?
Rick Barnich