Part Number: TPS54331 I have designed a DC to DC that has input of 12 to 18V and output at 8.5V.
Following is the schematic used
I am getting the desired result but when I measure the output, I am getting the following result
The output rise…
Part Number: TPS54331 Hi team,
On the datasheet, the calculation of compensation component is depicted. What is alpha mean in the equation 21?
Best regards,
Shunsuke Yamamoto
Part Number: TPS54331 Other Parts Discussed in Thread: TPS54531 Hi team,
Are there any pin-compatible devices with TPS54331 whose current limit is higher than TPS54331?
Customer evaluates TPS54331 in their system, but they found that the inrush…
Part Number: TPS54331 Other Parts Discussed in Thread: LM66100 Hi all, I have a setup with a TPS54331 configured to 5V output and want to OR between a primary(24V) and secondary (5V USB) power sources. The secondary 5V-usb source in only used during maintenance…
Part Number: TPS54331 Dears,
Customer use the TPS54331,the input is 24VDC,output is 5VDC.
1.Now they find when the C180 is 8200pF and C178 is 68pF and C172 is 22pF,the output waveform shows ladder,pls find attachfie for waveform#1.
2.When the C180…
Part Number: TPS54331 Hello,
In one of the applications, I am using TPS54331D which I need to step down to 5V from 12V and 24V based on the input voltage provided. The buck converter works fine in 12V input, but when I am increasing the voltage to 24…
Part Number: TPS54331 Hi,
We’ve had 4 instances now with our product in a particular geographical location whereby the 3.3V supply circuit has failed. On review of the failures, the catch diode has failed short and, in 3 units, the TPS54331 was also…
Part Number: TPS54331 Other Parts Discussed in Thread: TPS54561 , Hello TI,
why there is 0.8 in eq(9) of tps54331 datasheet? it's different from tps54561.
Part Number: TPS54331 Other Parts Discussed in Thread: TPS62933 Dear sir:
We use tps54331 to design a circuit with an output of 14.3V
Our input power supply is a 4s2p battery pack with a voltage range of 14.4V ~ 16.8V.
The circuit diagram is as…
Part Number: TPS54331 Hi
I have a situation where I have to sources that feed a single 5V rail.
One is the output from a boost converter that feeds of a battery. The other is a TPS54331. Is there any problem with backfeeding the output? VIN will be…