Part Number: TPS54341 Other Parts Discussed in Thread: TPS54302 , TPS54308 , , TPS54240 , TPS54260
Dear team,
May I know what is TPS54341/ TPS54302/ TPS54308 of maximum duty? I saw datasheet said that they can operate around 100% duty cycle, but there is…
Part Number: TPS54341 Other Parts Discussed in Thread: TPS564201 , LMR14030 , , TPS54260 , LM76003 , LM73605 , TPS54340 , LMR23630 , LM43603 Hello TI,
I used a TPS564201 (DCAP) DC/DC Convertor with my previous design to power a GSM/LTE Module. The transient response…
Part Number: TPS54341 Hi,
We designed a 22-30 V to 6V converter using the TPS54341, please note the schematic below. The inductor value is 3u3 and the voltage drop of the diode nominally is 0.55V.
The converter correctly outputs 6V under 4 Ohms of load…
Part Number: TPS54341 Hi,
We are designing a 22.9 - 29.4V to 6V converter using the TPS54341. The device functions as expected on a 4 Ohms load (1.5A), however on a 2 Ohms load(3A) the voltage drops to about 4.2V. The maximum signal appears to reach the…
Part Number: TPS54341 We are using TPS54341 in our application. After power fail, PWRGD signal is going LOW for 10 seconds and after that it is reading HIGH. Where as VIN, EN, FB and SW pins are LOW. Can anybody tell us the reason and how to make this…
Other Parts Discussed in Thread: TPS54341 We failed ECE Reg 10 for Radiated Emissions in Europe by 4 dB @ 258 MHz. After probing around, most of the radiation was coming from the TPS54341 switcher. The solution was decreasing the DC switching frequency…
Other Parts Discussed in Thread: TPS54341 Hi all,
i please need your help on the TPS54341 DC-DC-Converter. In the datasheet there is no hint on a maximum value that is allowed for the output capacitor. Can i place 220mF there as a buffer in parallel to…
Other Parts Discussed in Thread: TPS54541 , TPS54341 Hi Team,
Our customer would like to know about current limit of TPS54541 and/or TPS54341.
If the output of this device is shorted at the following conditions, can this device prevent the destruction…
Other Parts Discussed in Thread: TPS54541 , TPS54341 , TPS54260-Q1 Hi Team,
Our customer is requesting us to provide “Open- short test between the each pin of TPS54541 and/or TPS54341(FMEA)”.
Because, they would like to base on a security standard…
Other Parts Discussed in Thread: TPS54341 , TPS54340 Hi there,
Is there are any way to get our hands (located in Canada) on 75 pcs of TPS54341 by the middle of January for our first 25 boards coming into production? In prototypes we use almost identical…