Part Number: TPS54360 Hi Teams,
The customer is using TPS54360 to design the robot power board. Could you please help check if the schematic and layout are reasonable.
TPS54360.zip
Thank you for your support
BR~
Part Number: TPS54360-Q1 Hi,
I am using TPS54360-Q1 DCDC converter in my circuit. I connected 274KOhm resistor across RT pin and GND which sets the switching frequency to 354KHz as per datasheet switching frequency formula.
FSW = 92417 / RT(Kohm)…
Part Number: TPS54360 I need a power supply that runs on 35VDC (34V-36V) and outputs anywhere from 1.2V to 32V. I need it to be able to deliver at least 1A. I need it to be as efficient as possible (within reason, and cost is less important) and I need…
Part Number: TPS54360 Tool/software: Usually there should be 'COO: XXXX' or 'Made in XXXX" on the top left corner, right below the 'TEXAS INSTRUMENTS'.
Is it normal to be completely blank, not showing any COO information here?
Part Number: TPS54360 Tool/software: I'm trying to build a circuit using TPS54360. I plan to use 24V as input and 5V as output, but I want the GND of the input and output to be separated.
Is it okay to use the GND of the input and output separately…
Part Number: TPS54360 Other Parts Discussed in Thread: TPS543620 Tool/software: Team,
Could you please help to share me the Coefficient of Thermal Expansion(CTE) data of TPS54360? Thanks!
Best,
Qiang
Part Number: TPS54360 Other Parts Discussed in Thread: TPS543620 Tool/software: Hello Team,
We found some TPS54360 PIN2, 5 and 3 crack issue on our board. So we are doing some layout investigation. Below picture is the example layout in our D/S and…
Part Number: TPS54360 Tool/software: In my design from 48V to 12V configured with a 33 uH inductor the diode B560C is burned in few cases from more than one thousand. Tests and simulation do not led me to real cause. Can I find a way to replicate it?…