Hi Srinivasu
Line and load regulation for 5V is available in t he datashe et under section 8.2.1.3 Application Curves. Data is not available for 3.3V and 1.8V with us. You can test your solution on TPS54360EVM- 182 to get those plots
Thank You
Regards
Onka…
Part Number: TPS54360EVM-182 Hi,
I recently got back my design and there is some ringing in the supply. I watched the video from Dave Priscak and Robert Taylor and now I understand why. Is this reference design and Board available?
Thanks! -James
Part Number: TPS54360EVM-182 I have a customer attempting to use the TPS54360EVM-182 EVM. Upon powering up, customer is observing nothing at the output.
VIN: 12V, EN: open
Device is pulling 300mA with no load.
No activity at the output even after applying…
Hello,
Your layout looks good, it is a bit tight but overall similar to the TPS54360EVM-182.
Please probe SW node with an oscilloscope, this will help check if the converter is operating stable.
Also what component is getting the hottest? Is it the diode…
Other Parts Discussed in Thread: TPS54360EVM-182 Hello, all
Now we are evaluating TPS54360EVM-182, then would like to know the behavior when light load adopted.
Please see the enclosed report and feedback us your comment, in order to clarify this root cause…
Hi,
Yes the 2 x 47 uF capacitor has the nominal value of 94 uF. The datasheet mentioned voltage derating and temperature effect that reduced the "actual" capacitance value. Therefore the effective value is 58.3uF which is above the needed 29…