Part Number: TPS54361
Running to quite a bit of errors when simulating TPS54361 in spice for TI. Need help setting up the circuit and clear the errors. Errors seem to be internal to the part.
Part Number: TPS54361-Q1 Tool/software: Hello,
I was using your Power Designer tool, and i was wonderign if you have a similar solution to design a tree of power supplies instead of only a single supply.
Thank you
Davide Badoni
Part Number: TPS54361-Q1 Hello,
Is it possible to dynamically adjust the output voltage of the TPS54361-Q1 with a DAC as in application report SLVA861?
Thank you.
Anthony
Part Number: TPS54361 Hi,
My customer design requirement is
Vin:12V or 54V
Vout:3V3
Iout:0.6A
12V and 54V are big different, would like to know whether the device can support both 12V and 54V without BOM change, like inductor/compensation circuit…
Part Number: TPS54361 Hi,
How to find CMOS/BIPOLAR/BICMOS for the ICs which don't have information on datasheet or in website. For Example, IC TPS54361 doesn't have information on fabrication details. Kindly provide which fabrication technology is use…
Part Number: TPS54361 Tool/software: WEBENCH® Design Tools Im looking for the work bench simulation carried out on this device
How do i find it on E2E
Cheers
Colin
Part Number: TPS54361-Q1 Hello,
I guess the output current of a TPS54361-Q1 supply circuit will be reduced when the output is shorted to GND because of the TPS54361-Q1's switching frequency foldback function, but how small can the output short-circuit…
Hi Colin:
The maxim voltage of TPS54361 is depend on the process, so we don't have voltage withstand infomation as well as LM5576-Q1. cause it is not only internal mosfet need handle the VIn voltage but also the internal control circuit , driver. So…
Part Number: TPS54361 Can I bypass the input voltage to output when input voltage reaches to 30V using a Bypass P channel MOSFET. Or any other logic to implement this is welcome.