Part Number: TPS54361-Q1 Tool/software: Hello,
I was using your Power Designer tool, and i was wonderign if you have a similar solution to design a tree of power supplies instead of only a single supply.
Thank you
Davide Badoni
Part Number: TPS54361-Q1 Hello,
Is it possible to dynamically adjust the output voltage of the TPS54361-Q1 with a DAC as in application report SLVA861?
Thank you.
Anthony
Part Number: TPS54361-Q1 Hello,
I guess the output current of a TPS54361-Q1 supply circuit will be reduced when the output is shorted to GND because of the TPS54361-Q1's switching frequency foldback function, but how small can the output short-circuit…
Part Number: TPS54361-Q1 Other Parts Discussed in Thread: LM5576-Q1 , TPS54361 Could you confirm if the TPS54361QDPRTQ1 device can withstand an 80V input transient for approx 100uS .
Thanks
Regards
Colin
Part Number: TPS54361-Q1 Hi Team,
There is a good new that we could DIN TI product!
Please help suggest products that meet the following specificationsTHX
Spec:
DC-DC Synchronize Jeter for good EMI Can 4V~18V or ~ to 36V input Can 0.9V output…
Part Number: TPS54361-Q1 Tool/software: WEBENCH® Design Tools All my designs have become volatilized. When I try to open them it starts from the beginning. In the list of designs all appear, but when opening them is as if they did not pipe anything, part…
Part Number: TPS54361-Q1 Hello,
We are going to use TPS54361-Q1 for an Input Voltage range of 36V-72V and Vout = 12V. In the functional diagram, we didn't find any LDO or a mention of a how a regulated power supply is generated for the logic circuitry…
Part Number: TPS54361-Q1 Hello All ,
In the attachment diagram, added is a design I am working on. Design of SMPS for Automotive applications (Vbatt - from 12V to 48V). At the loads at the Vout is the ECU (Electronic control unit) which has many loads…