Hi Tagore,
Since the devices listed above are supported by different applications engineer, could you please create new separate threads for each device? Thanks! I will close this first.
BRs
Lucia
Part Number: TPS54386-Q1 Other Parts Discussed in Thread: TPS54386
Hello
Regarding the TPS54386-Q1, the buyer is requesting a response from the supplier.
Currently I am using 3.3V output for SW1 part.
During the load test, when a load of about 1.6A…
Part Number: TPS54386-Q1 Other Parts Discussed in Thread: TPS54386
Hello
Regarding the TPS54386-Q1, the buyer is requesting a response from the supplier.
Currently I am using 3.3V output for SW1 part.
During the load test, when a load of about 1.6A…
Part Number: TPS54386-Q1 Greetings,
I have a problem with large output voltage ripple in any L-C combination. ( Load 0.6 - 2 A)
If i change the input voltage to 12V, then the output ripple is minimal with the same configuration.
What could be the…
Part Number: TPS54386 dear
TPS54170+ TPS54386TPWPRQ power swith frequency show as bellow
TPS54170+TPS54386TPWPRQ EMI fail and ADI LT8530 pass, is there solution about reduce EMI radiation? thanks in advance
Part Number: TPS54386-Q1 dear
TPS54386TPWPRQ1, when will the chip enter the Steady state and skip? is there any way to force it to enter the steady state mode? Our load current is relatively small. At present, sometimes, products switch back and forth…
Part Number: TPS54386 Tool/software: WEBENCH Design Tools Hi,
Since this thread was older, I'm curious if the part TPS54386 added in WEBENCH tool yet? Particularly, webtool didn't show up any alternate design related to IC & no option to check dual outputs…
Part Number: TPS54386-Q1 dear
TPS54386TPWPRQ1, when will the chip enter the Steady state and skip? is there any way to force it to enter the steady state mode? Our load current is relatively small. At present, sometimes, products switch back and forth…
Part Number: TPS54386 Hello TI
If you connect the Raspberry Pi 5V line to SW1 of the TPS54386, it turns off after 2-3 seconds.
The 12V supply is supplied by the power supply and is displayed on the power supply. The current turns off when it reaches about…