Part Number: TPS54386EVM Other Parts Discussed in Thread: TPS54383EVM , LM60440AQEVM
Hi Team,
Could you please send the Altium, OrCad,... Design Files of TPS54386EVM and/or TPS54383EVM to me?
Or of PMP4961....?
Thanks.
Christos
Part Number: TPS54386EVM Customer would like to do the simulation for the loop gain/bode plot with real selected components. As we know, the capacitance losses with ceramic need to be considered with DC bias voltage. On the TPS54386EVM, we see there is…
Very Thanks.
However, On the TPS54386EVM board, all of the capacitors are using MLCC type. and its phase margin looks ok. I'm wondering to know if it has used the derated value for these MLCC capacitors or not?
In the TPS54386EVM, the calculated resonant…
Part Number: TPS54386
Dear sir, We are in the middle of designing a product prototype which uses TPS54386PWPR for a dual power supply, Vin 12V to Vout 5V & 3.3V with maximum load current 2A each. But we are facing a problem in getting output- 5V and…
Other Parts Discussed in Thread: TPS54386EVM , TPS54386 , LM317 hello!
My PCB include the power circuit the same as TPS56386EVM,the diffrerents are:the power supply is +5V,the VOUT1 is +1.8V while the VOUT2 is +3.3V. In VOUT2 part,I cut R10.
When I disable…