Thanks, Britton,
I have one more question:Why does the VIN to SW described in the datasheet have no limit to the negative voltage ( MIN ), which is also written in other datasheet like TPS543B20.
The following is the TPS543C20 sdatasheet:
Part Number: TPS543C20 Other Parts Discussed in Thread: TPS543B20 , , Tool/software: Hi Team,
I am using TPS543C20RVFT for Vin=12V, Vout=0.75V and Iout=40A. Please verify the schematics for the same.
Regards,
Shifali N
0882.TPS543C20RVFT.pdf
TPS543B20_TPS543C20A_TPS543C20_Calculator_0…
Part Number: TPS543C20 Tool/software: Hi,
Please verify the schematics for Vin = 12V and Vout = 0.75V. Sense pins of regulators are connected to sense pins of IC, please verify if that part is correct.
Thanks
/cfs-file/__key/communityserver-discussions…
Part Number: TPS543C20 We are using the TI part TPS543C20RVFT in our design for generating 0.72V with 40A ( two stacked), since the output voltage is very low and there is an high current requirement, i worried about the power path loss. Below are my…
Part Number: TPS543C20 Hi,
1. Please verify the schematics and provide your feedback.
Vin - 12V, Vout -0.85V, Iout - 80A
/cfs-file/__key/communityserver-discussions-components-files/196/TPS543C20RVFT_5F00_2.pdf
Regards,
Nachiketh Karanth
Part Number: TPS543C20 I want to use the part 'TPS543C20RVFT' in my design, but the WEBENCH simulator not showing the this part for simulation. So how to simulate the 'TPS543C20RVFT' part in WEBENCH for my requirement?
Part Number: TPS543C20 Other Parts Discussed in Thread: TPS543B20 , , Hi Team,
I am using TPS543C20RVFT in my design and the design parameters mentioned as below:
Vin=12V
Vout=0.85V
Iout=40A
I have attached the circuit design and would like to get it reviewed…
Part Number: TPS543B20 Hi expert,
My customer has some questions on 5V input application.
If the Vin is 5V, what is the output of BP pin?
Following from question 1, is there any limitation to use 5V for input?
Thanks,
Oliver
Part Number: TPS543C20 I need a rad hard part with the same or close to the same specs.
I need to make 22 Amps at 1V from a 5V input in a small package area.
I have looked for Rad hard and the website diverts my search to commercial.
Thanks