Other Parts Discussed in Thread: TPS54418 Hi,
Now our customer is testing TPS54418 on theirtest board and then they can confirmed start-up failure sometimes. Can you check and give your comments if you can find some problem points into waveform and…
Other Parts Discussed in Thread: TPS54418 Hi,
I made a schematic of circuit regulator on SwitcherPro with this specifications: Vout = 1.1V, Iout = 0.5A, Vin min = 4.7V, Vin max = 5.2V with the regulator TPS54418.
But I need to use the inductor from…
Other Parts Discussed in Thread: TPS628502 , TPS628302 , TPS628512 , TPS54418 , TPS54318 Tool/software: Hi,
I am looking for drop-in replacement of these two parts.
1. TPS54218RTET
2. TPS54218RTER
Any suggestions for drop-in replacement solutions…
Part Number: TPS54519 Other Parts Discussed in Thread: TPS54418 , TLV62095 Hi
In our design, power input is USB voltage 5V, output is 4.2V, output current is 4A
Can I use TPS54519? I cannot simulate TPS54519 with Webench.
Are there other buck converter…
Hello user,
Here is a matter of what is specified and tested on our side for the TPS54418 regarding the Absolute Maximum Ratings that are set for EN pin.
We do not guarantee functionality over 5V for EN.
Unfortunately it is not a parameter in…
Hello Yuta-san,
Q1. I recommend you to read this other E2E post: TPS54418 as the same RT/CLK architecture as TPS57114C-Q1.
Q2. "If the RT/CLK pin voltage pulled HIGH due to clock source failure. What behavior of the TPS57114C-Q1 ?"
"On the other…
Part Number: TPS54618C-Q1 Other Parts Discussed in Thread: TPS54678 , TPS54719 , TPS54519 , TPS54478 , TPS54418 , TPS54618 Hi team
I searched on Ti.com and only found the TPS62816Q1 which is not pin to pin with TPS54618CQ1 just function similarly, so…
Hi,
These are internal values to the device that are fixed and not needed for any calculations. They are shown in the figure for completeness. The EA has a (very high) limited gain and a (very high) limited BW. Your C2 and R3+C1 compensation network…