Part Number: TPS54426 Hi
Because the MOSFET are in the converter, the spec only show the SW(low side MOSFET) max voltage=22V.
We want to know the high side MOSFET max voltage=?
Thank you!
Part Number: TPS54426 Other Parts Discussed in Thread: TPS74701 TPS54426 input is 4.5~18V, but on the SPEC, about Vreg5, is only show 5.3~5.7V when input is 6~18V.
customer wants to know the Vreg5 output when input is 4.5~6V, especially when input is…
Part Number: TPS54426 Other Parts Discussed in Thread: TPS54427 , TPS54428 Dear Team,
TPS54426 has the latch function for OVP and UVP. Does TI have any products of the same pinout without the latch function?
Best Regards, Hirokazu Takahashi
Part Number: TPS54426 Dear E2E,
TPS54426 show that the operated Vin range could be lower to 4V5, but why the test condition as VREG is only Vin,min=6V, not 4.5V.
Customer is confused if tps54426 can operate lower to 4.5V.
BR,
Jason
Part Number: TPS54426 Dear E2E,
Our customer is interested in the side effect if cap of REG pin is too small or large.
As I know, too small will cause Vreg voltage unstable result in converter abnormal.
if cap is too large, the slew rate of soft start…
Part Number: TPS54426 Other Parts Discussed in Thread: TPS54326 Hello.
The following description is in the "Power Good" section of page-8 of SLVSAD6C (TPS54426).
"If the feedback voltage goes under 15% of the target value, the power good…
Part Number: TPS54426 Hello.
It takes time from the end of the rise of Vout until Power Good becomes high. Is it OK to use Vout during this time? Should I wait until Power Good becomes high?
Regards, Dice-K
Part Number: TPS54426 Hi,
I am checking the output voltage accuracy. Is there information on how much line regulation and load regulation will be? (specification) Input voltage: 5 V Output voltage: 0.925 V Output current condition: 3A, 2A, 1A
Best regards…
Part Number: TPS54329E Other Parts Discussed in Thread: TPS54426 Hi team,
Customer cannot keep input capacitor as >10uF, which is the recommendation. The value is 6uF(effective input capacitance). Is it acceptable for the device?
They have same question…