Part Number: TPS544B25 Hi,
I have the TPS544B25 on a board of mine and am trying to reconfigure the eeprom so that I set a correct output voltage, scale, ovp, etc...
Right now I am using an aardvark to communicate to the IC, but I am not getting…
Part Number: TPS544B25 we found TPS544B25 has CML error after power up, TPS544B25 drive the SMBus alert signal to low. The CML error shows "Invalid Cmd" and it can be cleared. I wonder whether there is same error on TPS544B25 demo board, then we can be…
Part Number: TPS544B25 For TPS544B25, can we set the boot voltage to 0.72V?
Because datasheet only shows Vboot =0.8V when Rset is 8.66kohm.
Can we set the Vboot is 0.72V and what Rset we should choose?
Part Number: TPS544B25 Dear Sir,
Sub : TPS544B25 Regulator with external Sync clock,
Regulator input, output and current requirements. Input Volts = 4.0V - 6.0V DC Output Volts = 0.95V DC Max Current = 20A
Architecture : In our design we will power…
Part Number: TPS544B25 For TPS544B25, Is it necessary for CNTL pin to set a pull low resistor? If we can add a pull low resistor, how many ohm does TI suggest?
Part Number: USB-TO-GPIO I have 2 TI programmers that are connected to 2 TPS544B25 (on 2 separate but identical boards) with the same PMBUS address. How can I use TI Fusion Digital Power Designer software that is installed on the Windows PC to program…
Penn,
The TPS544B25 has 2 internal linear regulators that run most of the electronics within the device a 6.2V gate drive regulator (BP6) and a 3.3V analog and logic regulator (BP3) They are both run from linear regulators powered from the VDD input…