Part Number: TPS544B25EVM-681 Other Parts Discussed in Thread: USB-TO-GPIO2 , TPS544B25 Hello, USB-to-GPIO seems not to be available anymore and USB-to-GPIO2 is available now. Can TPS544B25 be evaluated with the USB-to-GPIO2 with no issues? what version…
Part Number: TPS544B25EVM-681 Other Parts Discussed in Thread: TPS546C23 , TPS544B25 Setup:
Setup 1: EVM connected to PC via PM bus adapter
Setup 2: EVM connected to External Device via I2C Bus
Explanation:
Setup 1: When I put below parameters…
Part Number: TPS544B25EVM-681 Hi, team
Customer wants to modify the evm's output voltage range 1~3V.
Could you tell how to modify the evm?
Regards,
Noriyuki Takahashi
Part Number: TPS544B25EVM-681 Hi,
I have a standalone c code in linux which reads the current from register 0x8C. The code always output 0xE007 even if no load register is connected.
Scenario 2:
I connect the EVM to the TI Fusion Designer application…
Part Number: TPS544B25EVM-681 I purchased the TPS544B25EVM-681 module to create a measure-based model for simulating the power rail eco-system for a high speed SERDES design.
In order to improve the model accuracy for the proper design of the on board…
Hi Peter!
Thank you for the answer, I think that I need to clarify my original question.
In the document named “Using the TPS544B25EVM-681 and TPS544C25EVM-681” the recommended schematic for feedback is:
I was asking about this 50 Ohm resistors…
Other Parts Discussed in Thread: TPS544B25EVM-681 Hi, Could you tell me about TPS544B25EVM-681? I'm trying to control by using the Fusion Digital Power Studio and USB Interface Adapter. However, Following screen appears and can not communicate. Could…