Part Number: TPS544C20 Tool/software: Hi Team,
Step 1: Provide the program to the programming vendor for flashing.
Expected Result: Program is successfully flashed.
Observed Result: Program was flashed without errors.
Step 2: After flashing, verify…
Part Number: TPS544C20 Tool/software: Hi,
There is abnormal operation intermittently.
Abnormal operation means no switching and no output.
It's occurred in 3 samples of 600 samples,
This symptom is duplicated at once of 10 times trying.
I checked…
Part Number: TPS544C20 Hello team,
Is there a write limit for the STORE_USER_ALL command?
If yes, what is the behavior expected when an instruction to write beyond that limit is given? (e.g. Accepts a command but returns an error)
(Background this…
Part Number: TPS544C20 Hello,
I have a few questions about TPS544x20 family (x = B, C).
Which registers can be written with the CNTL pin High (conversion enable)?
When is a new setting of the TON_RISE register effective after it's written with…
Part Number: TPS544C20 Other Parts Discussed in Thread: TPS548D22 , TPS548B22 , TPSM843B22 Hello,
I will not use the PMBUS communication (device configuration/control by the pins and no diagnostic). My product is battery powered. During standby, the…
Part Number: TPS544C20 Other Parts Discussed in Thread: TPS544C25 Hello,
My customer is considering designing a board that can use either the TPS544C20 or the TPS544C25 with only the BOM change.
Q1. TPS544C20 : BPEXT and TPS544C25 : VSET The function…
Part Number: TPS544C20 Hello,
I have dealing with two systems that program the device differently according parameters during execution.
Same version SW installed, same HW TI USB adapter and same project (xml) file but showing different parameters…
Part Number: TPS544C20 Other Parts Discussed in Thread: TPS544C25 Hello,
My customer was using the TPS544C20 on the customer-designed board.
They are trying to replace the TPS544C20 with the TPS544C25 without changing the PCB and peripheral components…
Part Number: TPS544C20 Hi Experts,
Our customer is looking for information about which nm Technology is inside TPS544C20?
I could not find information about this. Can you help?
Regards,
Marvin