Part Number: TPS544C25 Hi
We have used TPS544C25RVFT dc dc converter in our design but now we are faced issue in PGOOD pin which is output showing low but we are getting proper output voltage so please find below image and help to resolve this things…
Part Number: TPS544C25 Hello Team,
I do see some TPS544C25 triggering the over current events.
The current I can measure over PMBus is in the range of 20-24A while over current is set to 40A.
Thus from "steady" current I do not see the over current.…
Part Number: TPS544C25 In a previous post, I asked about the temperature coefficient on the TPS544C25 voltage regulation.
The response was: "While a typical part has a flat temperature response, any given part could have a small positive or negative temperature…
Part Number: TPS544C25 Other Parts Discussed in Thread: TPS546D24A I have a TPS544C25 that I'm writing VOUT_COMMAND to and the output voltage is not changing as expected.
VOUT_SCALE_LOOP is set to 0.25.
The VOUT_COMMAND value stored in NVM is 06AE…
Part Number: TPS544C25 Other Parts Discussed in Thread: TINA-TI Hi
We are planning to use below part in our design but meanwhile also we are checked simulation in TINA but showing some error in this simulation model so please help to get the resolve…
Part Number: TPS544C25 Other Parts Discussed in Thread: TPS544B25
This FAQ discusses how to set the Vout for TPS544C25, TPS544B25
Using Feedback Divider Network without PMBUS
If you want the converter to start to a default 0.84V as an example, here is…
Part Number: TPS544C25 Other Parts Discussed in Thread: USB2ANY , , IPG-UI Dear,
For the tps544C25, I would like to program some registers and load them to the EEPROM, such as the VOUT_COMMAND, via the USB2any debugger using the IPG-UI software.
Using the…
Part Number: TPS544C20 Other Parts Discussed in Thread: TPS544C25 Hello,
My customer was using the TPS544C20 on the customer-designed board.
They are trying to replace the TPS544C20 with the TPS544C25 without changing the PCB and peripheral components…