Part Number: TPS5450 Tool/software: Hi teams,
Mainly, when there is a sudden high current demand, there will be significant spikes in the 12V output ripple test, around 600mV. Some improvement plans have been made, but the results are not particularly…
Part Number: TPS5450 Tool/software: hi expert
1.Design and application conditions: U1 input voltage 29.2V±0.5V, U1 output voltage 5.4V, output current 3.5A max
2.The schematic diagram of the two schemes is as follows: Scheme 1:
Note: C52/C104…
Part Number: TPS5450 Tool/software: Hello,
My customer has some questions about the following application circuit of the TPS5450.
Q1. Would it be a problem if I use electrolytic capacitors instead of ceramic capacitors for C1 and C4 at the input?
Q2…
Part Number: TPS5450 Tool/software: Hi team,
Do we have any thermal test data with TPS5450 for below operation conditions? Is there any thermal risk if customer uses TPS5450 with below conditions?
Input: 24V
Output: 15V with 40W
Ambient temp: 70 degree…
Part Number: TPS5450 Tool/software: Hi Experts
I am using the TPS5450DDAR step-down converter to obtain 3.3V from 12V. It powers a set of LEDs and the microcontroller on the PCB. Please see the schematic below. The issue is that radiated emission peaks…
Part Number: TPS5450-EP Hi team,
could you provide the min and max value of below spec? Customer needs it to finish AVL. if no test data, simulation data also works, thanks a lot.
Best regards,
Yang
Thank you for using the E2E forum.
I will close this thread for now. If you have any further questions on this, please reply back and it will reopen for further assistance.
Part Number: TPS5450 Hi TIer
Due to the discontinued on TPS5450.
Do we have the pin2pin device which can use in mass production?
Customers need some pin2pin products to help normal production of mass production devices, and they will be revised in the…
Part Number: TPS5450-EP Hi
We found that there are many marks in the marking of one braid of this product. Could you please help confirm the reason
thank you.
Part Number: TPS5450-EP Hello
I am using TPS5450DDA in my project.
Input-28VDC
Output- 5V/5A
I have done above voltage with current.
1. Can I adjust output voltage 6.3V/5A with 28VDC input.
2. Who much adjust output voltage