Part Number: TPS54526 Hi, we are a group of Electrical Engineering students and we made use of WEBENCH in order to design the following power supply. It is not the first time that we made use of DC-DC converters.
When implemented on a PCB the 5.5V output…
Part Number: TPS54526 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models I am trying to use TI TINA to model a buck converter (TPS54526), which I obtained from exporting the WeBench file. However, I am not getting any desirable…
Part Number: TPS54526 Dear Team,
There is 1 resistor R3 connected for Soft start pin in application circuit.
What is the reason of this resistor.
Regards,
Prasanna G
Part Number: TPS54526 Dear Team,
We are planned to use 1.1V from 5V using TPS54526, IS it possible to generate since datasheet does not have resistor combination for 1.1V generation.
I have attached schematics , Please check this once .
Regards,
Prasanna…
Part Number: TPS54526 Dear Team,
We are using TPS54526PWP in our design, i have read sentence "Voltage feedback loop should be as short as possible, and preferably with ground shield".
But in our design we connected through plane instead of…
Part Number: TPS54526 Other Parts Discussed in Thread: TPS62130 Dear Team,
We are planned to use TPS54526 for generating 1.1V from Vin=5V, Is it possible?
If it is possible what will be the value of VREG if Vin=5V.
Is it possible to use PG (pull up with…
Other Parts Discussed in Thread: TPS54526 , TPS53319 , TPS53353 , TPS54020 Dear Team,
We are planned to use TPS54526 for generating 3.3V from 5V input,
As per datasheet it says 5A rating but i require 10A 3.3V , So can i use 2 IC in parallel to generate 3…
Other Parts Discussed in Thread: TPS54526 Dear Team,
What is the max output current we can get from TPS54526 when output =3.3V and input=5V.
As per datasheet it says 5.5A but i want to know Is this current rating changes with output and input voltage we…
Other Parts Discussed in Thread: TPS54526 Hi Team, I would like to ask about TPS54526. Is it possible to operate under Vin=4V if supply 5V for VREG5 externally? I understood the recommended voltage of Vin is 4.5~18V but it seems possible according to the…