Part Number: TPS54527 Tool/software: Dear Texas Instruments Customer Service Representative,
I'd like to ask question which include confidential information.
Could you share your mailing list?
Best regards, Takuma Horigami
Part Number: TPS54527
Hi,
Customer is using below circuit, and find the conducted emission at 12V——ADP is not met. Do you have any suggestions?
Thank you!
Part Number: TPS54527 Dears,
The spec of TPS52527 shows that output voltage is 0.76-6V,but customer design Vin 12V&Vout 9V,then they found the inductor is burned,rated about 25%.Detalis pls find below information:
1. Vin12V,Vout 9V,this design is…
Part Number: TPS54527 Other Parts Discussed in Thread: TPS54528 , We found that the TPS54527DDAR chip consumes too much power, with 12V input and 3.3V output. Even with all 3.3V loads removed, the 12V input has a self-dissipation of 30mA. Remove this…
Part Number: TPS54527 Other Parts Discussed in Thread: TPS54335A Hi,all
I now plan to use TPS54527 to output negative voltage -5V while the input is 12V. I want to know wether this part can satisfied this use.If it can,how to connect the vreg5 ,EN and…
Part Number: TPS54527 Hi team,
Do you have an efficiency curve more closer than the figure 7 in the datasheet (12Vin to 1.8, 2.5V, 3.3Vout) with the titled case in order to estimate junction temperature from case-top temperature?
Best regards,
…
Part Number: TPS54527
Customer would like to know about soft start of this part.
Please check attached file. We would like to know value with valration or equation of ? in attached file.
Regards,
Kura softstart.pptx
Part Number: TPS54527 Other Parts Discussed in Thread: TPS54528 , Hi TI
TPS54527DDAR this chip, we found that the power consumption is too large, 12V input and 3.3V output. Even if all 3.3V loads are removed, the 12V input has a self loss of 30mA. …