Part Number: TPS54540 Dear support,
in the last months we're facing a problem over a DC/DC stage based on TPS54540 regulator, it's mounted on a product landed the production some years ago but in the last batches we got a failure rate around 5%: the…
Part Number: TPS54540 Hi
The board is back and currently undergoing debugging. The circuit is related to the M.2 5G module.
The current issue is that AI analysis suspects power instability is causing 5G connectivity anomalies, which results in an…
Part Number: TPS54540 Hi TI
We use TPS54540 in an inverting buck configuartion. We have automated test systems that analyse the switching waveform of the DCDC converters, for verifying proper function. But on one out of 50 units, our inverting buck…
Part Number: TPS54540 Tool/software: Hi, For the IC TPS54540DDAR can we supply more than 8.4V to the ENABLE PIN to set " Under Voltage Lockout"? if so what is the maximum voltage we can supply.
in datasheet it is mentioned that when we exceed more than…
Part Number: TPS54540 I am TSR for NEC. I got the following question from NEC. Please answer it.
For TPS54540DDAR at Input 24V, Output 5V & 3.3V,
Customer is considering using it in a power supply circuit.
Looking at the data sheet, the thermal…
Part Number: TPS54540 Tool/software: attach the schematic. the issue is:
when the load is less than 0.7A, the Vout is working normally.
when the load is higher above 0.7A, the Vin will be pulled down to 4V, lead Vout can not output normally.
…
Part Number: TPS54540 Other Parts Discussed in Thread: TPS84259 , TPS54040A , TPS54060A , TPS5430 , TPS5450 Hi,
Good Day. I have a customer who is working with TPS54540 and TPS84529. Please see below his query for your reference. Thank you very much…
Part Number: TPS54540 Other Parts Discussed in Thread: TPS62903-Q1 Hi team,
My customer asked that can TPS54540 quick discharger when we remove the loading? they have one situation that will disable output loading and this moment would need to Vout…
Part Number: TPS54540 I am TSR for NEC. I got the following questions from NEC engineer.
For TPS54540DDAR at Input 24V, Output 5V & 3.3V,
Customer is considering using it in a power supply circuit.
Looking at the data sheet, the thermal resistance…