Part Number: TPS54540B Other Parts Discussed in Thread: TPS54540 , , TPS54340 Hi team,
Could you give me comments on following customer questions? They want to know more detail about difference between TPS54540B and TPS54540.
<Customer question>
…
Hi Samuel,
We did a cross-reference between TPS54540-Q1 EVM and customer’s board. We installed customer’s TPS54540, inductor (L10), output capacitor (C86, C87), diode (D16) onto EVM, set EVM frequency to 950KHz and used the same comp values. We connected…
Hello Dhimat,
We do not have any dual switchers with integrated fets rated to 40V.
Our dual integrated fet switchers, like TPS55386, are only good to 28V.
For single switcher with integrated fets see:
TPS54540 TPS54040A TPS54140A TPS54240 TPS54340…
Hi Antonella,
I run the schematic through the calculator and it looks ok.
3823.Copy of TPS54360-361FAMILY_CALC_TOOL_REVE.xls
Do you have the waveform of the SW node, VIN, VOUT at 2A and at 4A with the TPS54560-Q1? Also, do you have the layout of your…
Other Parts Discussed in Thread: LM22680 , TPS54540 , LMC555 Hi all.
Would you mind if we ask about LM22680?
LM22680 has the function of self synchronization. Is it possible to synchronize multiple DCDC (LM22680 and TPS54540)? If it is possible, Q1: Please…