Other Parts Discussed in Thread: TPS54550 , SWITCHERPRO I have a question about TPS54550.
Please tell us the data of loop response.
①Vin=12V
Vout=6.0V
Iout=4.7A
Fsw=250kHz
②Vin=12V
Vout=9.0V
Iout=3.6A
Fsw=250kHz
Our customer tries to use Switcher…
Since I could not find the previous data, let me recount as best I can from memory.
As stated above, When TPS54550 starts into a pre-bias condition, the feed back voltage is higher then the SS voltage (the non inverting error amp input is the lower…
Other Parts Discussed in Thread: TPS54550 The stated max value for this test on page 5 of the datasheet is 0.5v. When I do this test I get about 0.8v. Can you tell me the proper way to perform this test to get a typical value? The data sheet says that…
Other Parts Discussed in Thread: TPS54550 , SWITCHERPRO Hello. My customer is currently in use TPS54550, I have gotten a question about this product .
So , I have a question about TPS54550.
<Question>
Q1:Does this device will be able to use the Switching…
Other Parts Discussed in Thread: TPS54550
Hello.
My customer is currently in using TPS54550,now.
I have gotten a question about this product .
So , I have a question about TPS54550.
<Question>
For the following graph , what happens in the VIN = 4.5V…
Hi John, were you able to find the switcherpro image ? I have also tried to use Webench too, but the TPS54550 part is not supported, and the Spice model seems to be encrypted.
Is there likely to be support for the TPS54550 in Webench ? Maybe I should…
Other Parts Discussed in Thread: TPS54550 Hi,
In TPS54550, if am not using Soft start or enable function, can i left the pin floating.
Want to confirm this.
TIA
Other Parts Discussed in Thread: TPS54550 Hi,
Am using TPS54550. For Vin=5V(4.5to5.5) ; Vout=1V (50mV ripple) ; Freq-700KHz, am getting a max efficiency of just 81% at for 4.7uH (Tunable).
Please help me in tuning the circuit to achieve a min of 85%…
Other Parts Discussed in Thread: TPS54550 , SWITCHERPRO In reviewing the data sheet of the TPS54550 device it would appear the load current could go to 0 A with the regulation being within 0.1% with a Vin of 12V. Yet when I run SwitcherPro it doesn't allow…