Part Number: TPS54560-Q1 Other Parts Discussed in Thread: TPS54560B , , LM61495-Q1 , LM61440-Q1 , LM61460-Q1 , LM61440 , LM61460 , TPS54560 , TPS54560B-Q1 Dear Support Team,
my company has succesfully used the TPS54560B IC in the design attached for a 12V to 5V…
Peter
I understand your frustration in needing to know the latest information but the feedback I have received is that you will need to use the info on ti.com as the latest info on these devices. I did ask exactly when info gets posted after a PCN expired…
Part Number: TPS54560 Hello TI,
Really need help with this, we have the TPS DC-DC with variable voltage output (5-50V) and on top we have a PWM circuit for voltage control (dimming).
At high power loads or any load actually, the efficiency is really…
Part Number: TPS54560 Hi Team,
Can you please check and advise with following request:
"
We use TPS54560 integrated in our power cards. However, the input voltage in our product is up to 55V due to the battery. When we draw high currents at these…
Part Number: TPS54560 Hi Team,
What the Value of Vds of TPS54560 is safe?
Vds of TPS54560 Datasheet is 65V, and customer spec is 52V(80% of 65V).
After I helped the customer to test, the Vds of Hide side MOS is 61.6V, and the VDS of low side MOS is 61…
Part Number: TPS54560-Q1
Hello,
I built a test board for TPS54560-Q1 base on schematic below. and when I power it on, the output voltage is < 1V.
I want to konw what is the reason it behaves this way. I checked every connections, the voltage on pin…
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: TPS54560 Hi
Standby power consumption is now tested at 10mA. Is there any good suggestion to reduce power consumption?Thanks!
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: TPS54560B-Q1 , We are using the TPS54560-Q1 down-converter in our design pretty successfully, however a new set of boards arrived and about a 1/3rd of them the device blew up when applying power …
Part Number: TPS54560 I configured the circuit with TPS54560 .
50V battery input -----> 5V ,5A output
but , the VIN part burst at the moment of connection.
It works fine with 20V and 30V input...
It shows 4.5v to 60v input on datasheet.
What's wrong…