Part Number: TPS54560 We are facing temperature raise issue while output current is 3.2A , input & output ratings are given below.
Input voltage - 32 V ,Output voltage - 5V, Load current - 3.2A continuous load
The entire PCB temperature is raised…
Part Number: TPS54560 Hello TI,
This question is in relation to this post -> https://e2e.ti.com/support/power-management/f/196/p/960683/3550140#3550140
We need to do a bit of a redesign that requires a higher inductance. Our device would be sometimes…
Part Number: TPS54560 Tool/software: WEBENCH® Design Tools The design values for compensation Resistor & capacitors seem to mis-match. I am attaching my calculation sheet do let me know. Attaching my calculation sheet TPS54560BQDDARQ1.xlsx
Part Number: TPS54560 Other Parts Discussed in Thread: TPS54360 Hello,
I have designed a PCB that would take a 60V input and output a voltage from 5V to 50V depending on a digital potentiometer IC.
This is my 3rd/4th iteration of the board and it would…
Part Number: TPS54560 Hi Team,
I need graph for junction temperature vs voltage reference for 48V input.
see below reference image for 12V. I need it for 48V. and its output voltage will be 15V and 5V
Thanks.
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: LM25117-Q1 , LM5146-Q1 I'm using the TPS54560-Q1 Step Down DC-DC Converter the input is 24V the output is 5A/5V, do I need a fan or/and thermal pad to help cooling the device.
Part Number: TPS54560 Hi Ti,
I am working on TPS54560 with the below specs
Vin: 24V
Vout: 12.4V
Iout: 4.2A ~ 4.4A
The load resistor (3 ohm) is used to to draw contstant Iout at 4.2A to 4.4A, after few seconds the IC overheat at 150degC and faced thermal…
Part Number: TPS43061 Tool/software: WEBENCH® Design Tools Error message if we change the input range but beyond the limits, example shown below.
"Design cannot be created! Your preferred device does not work with the inputs you selected." …
Part Number: TPS54560 Hello E2E,
I would like to consult how to correct to select the inductor's saturation current.
The OCP of TPS54560 is fixed. Assume the maximum load current is just 1.5A and due to PCB size limitation, could user use the lower…
Part Number: TPS54560-Q1 Other Parts Discussed in Thread: TPS54560 , TPS54560B
My customer use TPS54560-Q1 in their power board. About one-sixth of the defective rate of trial-produced products. The Vin is 12V and the designed output is 5V, but the output…