Part Number: TPS54560B Other Parts Discussed in Thread: TPS54560 I'm using TPS54360-361FAMILY_CALC_TOOL_REVE.xls to design. How do I tell whether I should expect acceptable performance? I'm assuming the Small Signal sheet should show what to expect, but…
Part Number: TPS54560B-Q1 Hi,
l have designed a buck converter using TPS54560BQ with following specifications:
VIN : 48V
Vout: 24V @ 5 Amps
Continuous current at 24V : 2.5 Amps
Ambient temperature: 45 deg Celsius
Schematic is copied from Power designer…
Part Number: TPS54560B I'm using the translation function, so I'm sorry if the sentences are strange.
I'm thinking of making a DC60V→DC12V5A circuit referring to the design example DC60V→DC5V5A.
How was R esr = 1.67mΩ used in Equation…
Part Number: TPS54560B Other Parts Discussed in Thread: TPS54560 , https://drive.google.com/file/d/1Wl4QeXNmdnPTEHqAqKZgJTs-wI_8RmnF/view?usp=sharing
Too much heat is generating over the board and the IC Temperature goes beyond 94.2 Degrees with normal…
Part Number: TPS54560B Other Parts Discussed in Thread: TPS54560
Hi Team,
In our customer's application, the TPS54560BDDA drops out/locks out when the input voltage is greater than 4.5V for an output of 5V. Please see the details of his inquiry below…
Part Number: TPS54560B-Q1 Hello TI, I have designed a circuit using TPS54560BQDDARQ1, DC-DC converter. Operating input voltage is 24V (From manual SMPS). We designed circuit to get output voltage is 3.3V . The circuit is same which was given…
Part Number: TPS54560B-Q1 Hello
Are the following devices Isolated or Non isolated:
TPS54560BQDDAQ1 and TPS54560QDDARQ1
What does the B stand for?
Best Regards
Nigel
Part Number: TPS54560B-Q1 Hello,
My customer wants TI review of their TPS54560B-Q1 circuit design.
Could you please review the following circuit design?
- The input voltage is planned to be 12V or 24V, and up to 36V can be input.
Thank you.
JH
Part Number: TPS54560B Hi there, I was reading about this chip and how it has a current limit to it. I am confused if I am able to set a current limit on the chip or if the current limit is just internally set to around 9A (as shown on page 5 table 6…