Part Number: TPS54618-Q1 Hi there,
as shown on the datasheet, FB voltage is 0.8V, does TPS54618 support stable 0.8V output if i connect the FB directly to Vout?
BRs,
Shubiao
Part Number: TPS54618-Q1 Vin: 3.3V, Vout : 1V, Load Max: 3.2A, Initial load: 20mA
Observed irregular start-up voltage at the output, please find schematic and waveform below. Please help me understanding why this behavior is observed
Part Number: TPS54618-Q1 Hi,
My customer would like to know what is the difference between TPS54618-Q1 and TPS54618C-Q1?
If my customer is just in sample run, can we use TPS54618-Q1 first?
Thank you.
Part Number: TPS54618-Q1 Hi team,
Would you please check if TPS54618-Q1 is ok to use boot resistor? or can only use snubber?
Here is a post regarding TPS57114-Q1, we don't recommend to use boot resistor for TPS57114.
So I would like to double check…
Part Number: TPS54618-Q1 Hi,
We are using this IC to generate 0.9V & 1.05V from 3.3V
We are using 100nF as BOOT CAP. Need to know what is the boot cap requirement with respect to temperature variation.
Our system operates in -40C to 105C. What is…
Part Number: TPS54618-Q1 Tool/software: WEBENCH® Design Tools Dear Team,
My customer will have 600uF*2 at the output.
So I would like to use Webench to find the suitable compensation value.
But the webench only mention the phase margin is not enough,…
Part Number: TPS54618-Q1 Hi TI fellows, could you provide the worst case leakage current at the VSENSE input for the part TPS54618QRTERQ1? I understand that it is not stated on the datasheet. However, I need this value to calculate the worst-case output…