Part Number: TPS54618-Q1
for th TPS54618-Q1. How do I do remote sensing?
Will the following have instability problem?
On the same PCB, about 6”~8” max from the POL.
Part Number: TPS54618-Q1 I am designing TPS54618-Q1 into an application. I wonder if two TPS54618-Q1 can do load sharing. If yes, how to do the load sharing? Will the following work?
Part Number: TPS54618-Q1 Hi team,
My customer designs TPS54618-Q1 enable which connects to EC and also pull down to ground through 100k ohm.
I know there is a pull up current in enable pin which is 1.9uA, if EC is no function now, the enable pin should…
Part Number: TPS54618-Q1 Tool/software: WEBENCH® Design Tools Hi TI experts,
When I used the WEBENCH to simulate phase margin, I see the results showed significantly different from different Iout with other parameters were totally same.
But this result…
Part Number: TPS54618-Q1
Hi, Customer wants to reduce the feedback and RT resistor value. (Because of the disturbance noise measures) Could you tell me the acceptable recommended value or range? Currently, customers are considering the following changes.
RH…
Other Parts Discussed in Thread: TINA-TI Hi,
There is a transient simulation model for buck TPS54618-Q1 available on TI webside but no AC simulation model. WEBENCH allows the transport of simulation model to TINA-TI but only transient analysis.
Is it possible…
Part Number: TPS54618C-Q1 Other Parts Discussed in Thread: TPS54618 , TPS62816-Q1 Hi TI guys,
Could you help to confirm the difference between TPS54618 C QRTERQ1 and TPS54618QRLBRQ1?
What's the meaning of C above?
Part Number: TPS54618 Other Parts Discussed in Thread: TPS62816-Q1 , TPS54519 , TPS54678 , TPS54719 hi team:
my customer sourcing one device as below request, can you help to confirm and promote ? tks in advance.
1. p2p with TPS54618
2. I max load >5A …