Part Number: TPS54622 Other Parts Discussed in Thread: UCD9090A Hi
What is the maximum voltage the EN pin will rise to when left floating and device is on
Thanks
Faizul
Part Number: TPS54622 What is the maximum ambient operating temperature we recommend for the TPS54622? I see it has a 150C Tj limit, but typically this is much higher than what is allowed (and took qual testing data on) for ambient... I can't find this…
Hi Elleen, Thanks for your response, Kindly confirm that the APP Note Calculator can support TPS54623RHLR. Over in the Excel sheet it was mentioned that this file supports the Below mentioned parts only.
TPS54218
TPS54318
TPS54319
TPS54320
T…
Part Number: TPS54622 I'm struggling to make complete sense of section 7.4.3 in the TPS54622 datasheet.
- What is the minimum VOUT for 100% duty cycle operation when PVIN and VIN are tied together?
Other Parts Discussed in Thread: TPS54622 , TPS54821 Dear fiend,
I am using a TPS54622RHLR 13.0V-17.0V to 12.00V @ 5.0A attached scheme.
My load is a motor with starting peak current of 10A for 200ms and 5A rated current.
Every time I'm trying to turn…
Part Number: TPS54427 TPS54427 support,
I tried simulating a load transient with TPS54427, and it doesn't allow any change to the load current. It seems to fixed at 10% to 100%.
If you open the settings for the load, you'll see () instead of "I1"…
Other Parts Discussed in Thread: TPS54622 Hi,
We use a DCDC chip TPS54622 failure , send your company Failure analysis is EN pin EOS failure,see attachment。
This is our circuit,
Our system requires the TPS54622 to start after the -5v and +5V start, so we …
Other Parts Discussed in Thread: TPS54622 How can the vout of the TPS54622 be trimmed +/-15% (via DAC or MCU) without triggering the over or under voltage protection as the VSENSE is set between 92% to 106%?
regards
Madhuri