Other Parts Discussed in Thread: TPS62130 , TPS543320 , TPS562203 , TPS54625 Hello!
I am looking for an alternative to the LTC3601EMSE#TRPBF. Does TI have something (preferably pin to pin) for this device? Nothing was coming up on the cross reference tool…
Part Number: TPS54625 Hello,
Some time ago we had trouble using TPS54625. A problem occured when we plugged a battery on our system and creating a short circuit between GND and VREG5 or VIN or VOUT (and disabling the component). We fixed it by doubling…
Part Number: TPS54625
see schematic below.
after power on,VOUT is 0.8V.
The wave shows Vin (blue 12V) shakes at rising edge.
Vout (yellow 2.5V) ends below 1V.
why tps54625 can't retry and get back to work normally?
Part Number: TPS54625
Hello
We have troubles using the TPS54625.
At first use or after a few uses, the VREG5 pin becomes internaly short-circuited with the GND and the output voltage stay at 0. A short-circuit between the GND and the Vout can appear…
Other Parts Discussed in Thread: TPS54625 Hello Everyone, I used the webench to create a 12v to 3.3v output @3.5A using the TPS54625,
When i power the supply up without any load, it outputs 3.34v, which is fine, but as soon as i put a load on it, it instantly…
Other Parts Discussed in Thread: TPS54625 The Circuit for generating 5.4V from 12V using TPS54625 is Generated from WEBENCH and the same circuit is used by me and the circuit is given below
After Giving 12V Input I am not seeing 5.4V(During No Load/ With…
Other Parts Discussed in Thread: TPS54625
I have generated the Buck Converter circuit using TPS54625 with 12V Input and 5.4V output in WEBENCH. And the same circuit is used in my design and circuit is shown above.
After giving 12V Input am Not Measuring…
Other Parts Discussed in Thread: TPS54625 , TPS54325 The TPS54625 has two pictures showing the thermal pad dimensions. Figure 16. of the datasheet indicates a 2.46 x 2.31 mm dimension as shown below (page 15.). The figure on the second to last page of the…