Part Number: TPS54678 Other Parts Discussed in Thread: TPS62869
Hi team,
just want to know min length of below package ( see red). customer requirement is 0.2mm. if do calculation as shown here, 3.1(2.9)- ( 1.65+/-0.1 ) - 0.5(0.3) * 2 = 0.15mm min…
Part Number: TPS54678 Hi, I'm currently using TPS54678 with input voltage, Vin=3.3V stepping down to output voltage, Vout=0.9V, designed with maximum output current, Iout_max=1.5A. I found that there is a glitch on rising edge of the switching waveform…
Part Number: TPS54678 Hi,
Can you provide the ROHS and MCD materials of TPS54678RTER to me via E-Mail?
I am not sure whether MCD, Material Composition Declaration, is the same as “Quality, reliability & packaging data download”. Thanks.
Regards…
Part Number: TPS54678 Other Parts Discussed in Thread: TPS62867 , Hi,
Can I get ratings for tDelay, tRamp, and tPG,DLY? I see these timings on TPS62867 DS and wanted them for TPS54678 for comparison.
Best,
Lucas
Part Number: TPS54678 Good morning,
What is the IC switching frequency tolerance while setting the switching frequency with a resistor?
In the data sheet, with a 82.5kΩ the range is stated as 400-600 kHz with a typical value of 500 kHz.
I have a…
Part Number: TPS54678 Good morning,
I am trying to understand the soft start timing formula in the datasheet on page-14.
If I understand it correctly, It says 2.2uA charges the SS from 0.15V to about 0.8V for the handoff of the SS voltage to reference…