Part Number: TPS546B24A Other Parts Discussed in Thread: TPS546A24A Hi,
I'm working on a new hardware design with multiple voltage rails - a <1V rail, 1.2V, 1.8V, 3.3V and 5V, operating from a 12V rail. The TPS546 series parts seem well suited for this…
Part Number: TPS546B24A Hi Expert,
Customer is using host BMC to configure TPS546B24A and found reading and writing to 1B registers confusing. The picture below describes “write word ” but there is only one byte. Also, what does the description (with…
Part Number: TPS546B24A Tool/software: The "Pin Functions" table in the datasheet says AVIN should be bypassed to "AGND". The layout guidelines section, as well as the device calculator spreadsheet, says to bypass to "PGND". Which is it?
Page 4:
…
Part Number: TPS546B24A Hi Team,
MSO USED- MSO58 TEKTRONIX
I am measuring ripple with coaxial cable.
Coaxial Cable have 50Ohm Impedance.
Is there any need to change the scope Input termination to 50 Ohm?
Beacuse when i am shifting the Scope…
Part Number: TPS546B24A Tool/software: Hi Sir,
We want to check wether is the Jitter Criteria in this IC?
what' percentage for Jitter?
Does other condition be checked? (If the bode plot is pass.)
Thank you.
Vivian
Part Number: TPS546B24A Hi Team,
I am using TPS546B24A.
Here is the setup information of Switch Node Measurment
VIN-12V
VOUT-1V
IOUT-10A
BW-1GHZ
NOTE- I did not see any Peak at 20Mhz BW so i am not sharing the snapshot of the measurment…
Part Number: TPS546B24A Hi Team,
I have creatted Power excel sheet (TPS546x24A_Compensation_Pinstrap_Calculator_Release20200120) for regulator used in design.I want to create .tifsp file for it.
Is there any user guide how to prepare tifsp file based…
Part Number: TPS546B24A Tool/software: Dear TI Team,
In the datasheet of TPS546B24A an example for output capacitor calculations with mixed capacitor types - ceramic and tantalum electrolytic is given.
We typically don't use electrolytic in our designs…
Part Number: TPS546B24A Hi,
For TPS546B24A, we found Vout command 0x0222 and get output voltage =1.066406V. Could you advis how to let 0x0222 transfer to 1.066406V? Do you have transfer fomula?
Thanks,
Part Number: TPS546B24A Tool/software: Hi Team,
I am getting Inductor Pk-pk Value as design waring. Shall I ignore it or change switching frequency to Lower to make pk-pk positive?
Many Thanks
Rajat