Part Number: TPS546B24A Tool/software: Hello,
My customer requested TI's review of the TPS546B24A design.
Please review their design below to see if there are any problems.
TPS546B24A.zip
Thank you.
JH
Part Number: TPS546B24A Tool/software: Hi,
My customer is attempting to make edits according to the previous schematic review (where I branched this thread from) and they wanted to double check a few issues they're seeing in the design calculator.…
Part Number: TPS546B24A Hi Team,
MSO USED- MSO58 TEKTRONIX
I am measuring ripple with coaxial cable.
Coaxial Cable have 50Ohm Impedance.
Is there any need to change the scope Input termination to 50 Ohm?
Beacuse when i am shifting the Scope termination…
Part Number: TPS546B24A Hi Team,
I have creatted Power excel sheet (TPS546x24A_Compensation_Pinstrap_Calculator_Release20200120) for regulator used in design.I want to create .tifsp file for it.
Is there any user guide how to prepare tifsp file based…
Part Number: TPS546B24A Tool/software: Hi Team,
When selecting an inductor, is it necessary to eliminate the saturation current of the OCP threshold selection inductor? If the inductor is selected based only on Imax, but at OCP, the inductor is deeply…
Part Number: TPS546B24A Hi Team,
I am using TPS546B24A.
Here is the setup information of Switch Node Measurment
VIN-12V
VOUT-1V
IOUT-10A
BW-1GHZ
NOTE- I did not see any Peak at 20Mhz BW so i am not sharing the snapshot of the measurment.
I looked into…
Part Number: TPS546B24A Tool/software: Hi,
I'm using TPS546B24A to generate 0.75V @ 12A from 12V supply in an evaluation board for an ASIC.
The issue I'm seeing is that when power on at 12V, it doesn't give the 0.75V output. In that case if I reduce…
Part Number: TPS546B24A Hi,
For TPS546B24A, we found Vout command 0x0222 and get output voltage =1.066406V. Could you advis how to let 0x0222 transfer to 1.066406V? Do you have transfer fomula?
Thanks,
Part Number: TPS546B24A Tool/software: Hi Team,
The 57h register doesn't seem to exist, but when trying to read the 57h register via PMBus it returns 14h. is this normal?
(1) Read 57h using TI dongle
(2) Read 57h using i2cget command in the AZ9074…
Part Number: TPS546B24A Tool/software: Hi Team,
We are facing voltage stablity issue with PIN Stap compensation value.
I have attached the excel sheet here for you review it seems everything fine in excel sheet .
we used PIN Programmed compensation…