Part Number: TPS546D24 Hi there,
My customer have been using TPS546D24 for one year. Some registers support NVM, which can store data as reset value. My customer would like to know the initial values of a virgin unit. Are they all 0b?
Thanks.
Part Number: TPS546D24A Other Parts Discussed in Thread: TPS546D24 Hello,
My customer requested TI's review of the TPS546D24ARVF design.
Please review their design below to see if there are any problems.
TPS546D24_N.pdf
Thank you.
JH
Part Number: TPS546D24 Hi Teams,
Is this product used widely? I noticed TPS546D24 released 1 year ago. The datasheet is selective disclosure. Do we need sign a NDA or other file?
We are estimating this product. The output voltage and current could cover…
Part Number: TPS546D24
questions about using TPS546D24 and full datasheet of this
hi dears i havve usung TPS546D24 as stackable 4 chip for 160 A output. but there is many questions about this chip: 1. there is little dates about PMBus threshold voltage and…
Part Number: TPS546D24 I have the TPS546D24 part on my PCB - that i am trying to gring -up and have hit a wall on this part.
My parameters are ;
Vout = 0.8V
I out = 26A
Freq = 550KHz
V resolution = 0.74V to 0.89V with 0.01 step
I need the strapping resistor…
Part Number: TPS546D24 Hi there,
My customer used TPS546D24 to supply a processor, the processor also works as a PMbus master to 546D24. They stored the loop config to NVM, and set the power up reset to NVM(reg_0xeeh = 0x00). They checked the bode plot…
Part Number: TPS546D24 I am trying to find out the recommended derating for the package and up to maximum current for the device. I see the maximum operating temperature for Tj is 150C which is also the absolute maximum Tj is 150C and the recommended…
Part Number: TPS546D24 Dear Sirs,
Trying to design a DC/DC buck for 2~2.5Vo@40A, my design targets a high precision output voltage (+-1mV @ 2Vo).
Can this IC fulfill these specs? Otherwise, there are other options on TI?
What about the recovery time…