Part Number: TPS546D24AEVM Other Parts Discussed in Thread: TPS546D24A Hey there,
My customer has this 2phase EVM in hand. What it the simplest way to make it single phase? Then, they will evaluate it with Fusion.
Thanks.
Part Number: TPS546D24A You have an eval board titled: TPS546D24AEVM-2PH which I purchased online.
How can I get the source codes for this design?
Please provide the link of the source codes of this EVM:
Regards,
Abdus
Part Number: TPS546D24AEVM Other Parts Discussed in Thread: TPS546D24A , TPS546D24 Hi there,
Does TPS546D24AEVM board could output a voltage higher than 1.5V? The inductor value on EVM board is 150nH, Does the Output support 0.6 V to 5.5 V at 80 A?…
Hi Timothy,
Is there a reason you want to use TPS546D24 instead of TPS546D24A? Because TPS546D24A is a newer version and we generally recommend it for new designs.
Timothy Tran2 said: Can I use pins-trap only to set 2x or 3x devices for current share…
JH Shin
For an estimate of the efficiency at a specific operating point, I would recommend using WeBench and matching the design components selection, then using it's efficiency estimator. This is important since efficiency is affected by external…
Part Number: TPS546D24A Hi Texas Instruments Customer Support
Thank you for your support, I have some questions for TPS546D24A, thanks.
Fixed frequency synchronous buck converter 2-phase evaluation module
www.ti.com/.../TPS546D24AEVM
1.…
Hi JH,
Please check out the TPS546D24A-2PH EVM: https://www.ti.com/tool/TPS546D24AEVM
This is a good place to start the design from. You can also generate a design on WEBENCH.
I also recommend you fill out the design calculator to determine key…
Did some extra testing.
I’ve changed inductors from 1uH to 150nH that I borrowed from TPS546D24AEVM-2PH. Added 2x1000uF bulk capacitors on 1V2 output as well as 2x1000uF on the 12V input rail. The result is exactly the same. The converter ramps up the…