Part Number: TPS546D24S Tool/software: Hello TI Team,
I am using the TPS546D24S in a single-phase, single-rail configuration with 12 V input and 0–15 A output . I am reading telemetry values through PMBus (READ_VOUT, READ_IOUT, READ_TEMPERATURE_1).…
Part Number: TPS546D24S Tool/software: We are using the **TPS546D24S** to achieve an **80A output** by **stacking two devices in a 2-phase configuration**.
We have configured the hardware according to the recommended reference design (as shown in the…
Part Number: TPS546D24S Tool/software: HI,
I am using TPS546D24S chip which can go up to 5.5V Vout (i changed the Vout max to 5v) but when i tried to change the Vout its giving me an error and showing that you could go maximum up to 3V.
Even…
Part Number: TPS546D24S Other Parts Discussed in Thread: TPS546A24A Tool/software: I am upgrading my system by replacing TPS546A24A to TPS546D24S as they are pin compatible; should i need to make any changes on the firmware programming in order to communicate…
Part Number: TPS546D24S Tool/software: Hello, We have Built 40Amps single phase PCB's which have 4 IC(TPS546D24S) in each PCB, After Configurations while power conversion without load output of some of the ICs were showing around 6.5V.
We have Checked…
Part Number: TPS546D24S Other Parts Discussed in Thread: TPS546D24A
Tool/software:
Hello Everyone,
I hope this message finds you well.
I am currently working with the TPS546D24S and noticed that the datasheet mentions the availability of simulation…
Part Number: TPS546D24S Tool/software: Hello,
Is it possible to adjust TPS546D24S output voltage on-the-fly using external DAC and not via PMBUS?
Thanks,
Itay
Part Number: TPS546D24 Other Parts Discussed in Thread: , , TPS546B24A Hi Team,
I am starting DVT of my board and want to test the transient and ripple of Buck Regulator(TPS546D24).
I just want to check which one be the right place to probe at the…