Part Number: TPS54719 I've implemented this power supply, and it works well for our purpose. The only issue is at startup there's a relatively high voltage transient on the output of the inductor, well before the soft-start ramp up begins. The upper cursor…
Part Number: TPS54719 Hi, Do these ICs use SMIC for manufacturing?
Function
IC Suppliers
MPN
SAP PN
BUCK
TI
TPS54719RTER
CNV-H-00000033
LDO
TI
LP5907SNX-1_8
VLR-H-00000101…
Part Number: TPS54719EVM-152 Other Parts Discussed in Thread: TPS54719 Tool/software: Hello TI Support Team,
I am working with the TPS54719 buck converter and have been analyzing the reference design (TPS54719EVM-152) schematic. I have a few questions…
Part Number: TPS54719 Other Parts Discussed in Thread: TPS62870-Q1 , TPSM8287A12 , TPS568215 Hi,
We are planning to use TI buck converter part no. TPS54719RTER as 3.3V Output powering VCCIO of two Xilinx FPGAs Spartan-7 (XC7S50-1FGGA484C, 2 qty)
VIN…
Part Number: TPS54719 Other Parts Discussed in Thread: TPS62811-Q1 , TPS628501 Hi,
We are using the TPS54719RTER buck converter for 1.8V and 1V for our application having two FPGAs (XC7S50-1FGGA484C, Spartan-7 series ).
Following is the requirement…
Part Number: TPS54719 Hi Team,
Normally I found that power good pins are pulled up to output of the switcher, but here it's connected to the Input source. As per mu knowledge Power good is enabled only after the output voltage came 50 or some% My question…
Part Number: TPS54719 Other Parts Discussed in Thread: TPS62867 , Hi, Pls review the attached schematics. Vout = 3.3V, Output Current required = 6A, Vin = 5V
Hi Yokota-san,
Thanks for bringing this to our notice.
You were seeing the issue because the Minimum on time of the device TPS54719 was being violated at 1.9 MHz at 5.5V Vin,0.9V Vout,3.5A Iout condition.
We have made changes to frequency ceiling…