Part Number: TPS54821 Hello,
I would like to use TPS54821 IC to generate -3V from 6 V for a kind of high current (5-6A) max 8A application.
For this purpose I have already ordered TPS54821-EVM-0049. I would like to check with this EVM that -3V is…
Part Number: TPS54821 Other Parts Discussed in Thread: TPS546E25 , TPS546D24A Tool/software: I would like thoughts on the potential for parallel-ing the outputs of up to six TPS54821 buck converters. The goal is to create a 0.8V 48A supply rail for an…
Part Number: TPS54821 Tool/software: Hi
I want to ues TPS54821 to generate 5VDC at VOUT, VIN=12V, due to the need for testing, I need to supply a external 5V directly to VOUT, VIN will be powered off, so can I do this? Would it damage the TPS54821?…
Part Number: TPS54821 Hello,
We are thinking to use relay for TPS54821’s Vin on/off.
Is TPS54821 broken if frequently power on/off?
We are need to “Slow-start” function, so for that frequently
Vin on/off Is required.
I will show you a reference…
Part Number: TPS54821 Other Parts Discussed in Thread: AFE7921 , Tool/software: Hi,
We used TPS54821 to power up AFE7921,but when I reset our AFE7921,the Voltage will drops.The AFE7921 power up must be follow Power-on sequence,the datasheet suggest…
Part Number: TPS54821
Hello TI Engineers,
Can I operate the TPS54821RHLR circuit as shown below?
Here are the details of the block diagram
1. The TPS54821 Circuit is designed for 12V Input Voltage and 7.5V Output Voltage
2. The same BUCK output…
Part Number: TPS54821 Other Parts Discussed in Thread: TPS54622 , , TPS548B28 , TPS53353 , TPS54KB20 , TPS56C215 Tool/software: Hi,
Do we have P2P with TPS54622 but with higher current(10A) devices regarding to TPS54622?
Thank you,
Yishan Chen
Part Number: TPS54821 Other Parts Discussed in Thread: BQ24133 Tool/software: Hello TI Engineers,
I would like your assistance with reviewing the layout of the TPS54821 circuit. This is a related to a previous post I made about introducing a reverse…
Part Number: TPS54821 Hello,
In my case i have problem with assembled from my design
Input 12V but output show 1V I followed WEBENCH® Designer and added a little custom
this my schematic
Thanks
Part Number: TPS54821 Hello,
In my design I use TPS54821 to convert from 12V to 8V.
Unfortunately the output voltage not stable around 2V instead 8V
Thanks