Part Number: TPS54821 Dear all
I am power system designer for Satellite.
I want to use the TPS54821 for the space.
So I did the TID(Total Ionizing Dose) radiation test.
When over the 12krad, I was failed.
And UVLO voltage was changed from 4V…
Part Number: TPS54821 Hi Sir,
Our customer have PWRGD turn low issue, we are check the schematic PWRGD pull high R is used the 10k,
If we are change to EVM suggest 100k, then Solve this problem.
what change the PWRGD pull high R improve this issue…
Part Number: TPS54821 Hello I'm using TPS54821 regulator in my project. I have used TI WEB BENCH Simulator and implemented my design, wherein it is showing very less ripple value. But practically I'm getting 100mV. I need ripple to be less than 50mV.…
Part Number: TPS54821 Dear All
I use the TPS54821 to design buck circuit 5V--1V, the schematic as below
when the no loading condition, the output voltage wave as below, it looks like wrong wave , can you help me what cause the result and how to…
Part Number: TPS54821 Tool/software: WEBENCH® Design Tools So here is my concern according datasheet of tps54821 it is recomended to put two 47uF capacitors for output ...atteched screenshot for reference now why can't i use one 100 uF capacitor instead…
Part Number: TPS54821 Hi Team
Our customer want to know the value of OVP
I can't find the value of OVP on the datasheet.
The spec of circuit as follow
Vin = 12V
Vout = 3.3V
Iout = 4.83A
What is the value of OVP, I would like to suggest to…
Part Number: TPS54821 Other Parts Discussed in Thread: TPS54620
Hi team, we recently discovered one faulty piece of TPS54821 after some time of operation. Behaviour is that DCDC does not work and PH pin seems to have 0.6Ohm to GND on un-powered board…
Part Number: TPS54821 Hi team,
my customer is using this device for a 14VIN, 5VOUT, 400mA nominal output design.
we are running into an issue whereby some of the devices are failing.
they noticed that the device did not load the source and did…