Part Number: TPS548A20 Hello,
My customer requests that the post below be removed due to company policy. They said that something that should not be posted on a public forum was posted.
Could you please help them?
https://e2e.ti.com/support/power…
Part Number: TPS548A20 hello all , i'm designing a circuit to regulate from 4s battery (14.8v) to get 3.3v , i need anyone to help me with the schematic and components value i need the circuit to give me current 13:14 using TPS548A20RVER , if you previously…
Part Number: TPS548A20 Hi TI Team,
I have used the buck converter TPS548A20RVET to generate 1.05 V for an Intel processor.
Design constraints:
VIN: 12 V
VOUT: 1.05 V
IOUT: 8 A
The Intel processor provides VCC_SENSE and…
Part Number: TPS548A20 Tool/software: Hi All,
I have a question about the Load Transient of the TPS548A20. Even in FCCM, does the switching period change temporarily at the moment the load changes?
When I checked the data sheet, it looks like switching…
Part Number: TPS548A20 Hello Sir/Mam
We are using TPS548A20RVET in our Design . We need to monitor it's Power good signal so it has to be connected to FPGA with IO Voltage 3.3V. As mentioned in Datasheet it has to pulled high with VREG(5V). So we…
Part Number: TPS548A20 Tool/software: Hi all,
When designing Cout, I understand that it is good to make Fp=1/2π√LC close to the corresponding value of Vsw.
According to Table1, when Vsw=600, 750kHz, Fz is 9kHz below.
I should select the inductor…
Part Number: TPS548A20 Tool/software: Hi,
One of my customers has a question about the TPS548A20. The design checklist shows 120us soft-start time, however, the SPICE simulation suggests a 4ms startup time.
Is there method in we are missing for…
Part Number: TPS548A20 Other Parts Discussed in Thread: TPS548A28 , TPS548B28 Tool/software: Hi,
I have customer looking into using this device, they had a couple of questions
1) Is “SLUSC78A –NOVEMBER 2015–REVISED DECEMBER 2015" the newest version…
Part Number: TPS548A20 Tool/software: Hi Team
Please find the attached Schematic in our design.
Our Requirement as follows:
VIN Min VIN max Output voltage Maximum current (peak) [A] 6.6 13.2 1.2V 15A Kindly provide the schematic review comments…