Part Number: TPS548D21 Hi,
We have designed a board using the TPS548D21 regulator. The current requirement in our design is 26A.
Under the thermal pad, we have provided 23 Vias of 18mil pad diameter and 8 mill drill size.
These via pads are masked and…
Part Number: TPS548D21 Other Parts Discussed in Thread: TPS548D22 Hi,
I use TPS548D22 to design a DC/DC: input is 12V, output is 0.6V, current is 40A. Because the lead time of TPS548D22 is 25W please help to check whether TPS548D21 can replace TPS548D22…
Part Number: TPS548D21 hello
Can you Review the schematic for below specifications?
VIN : 4.8 ~ 5.8V
Output Voltage : 0.85V (+- 0.025V)
Output Current : 25A ~ 30A
OP Temperature : -40 ~ 80℃
Regards.
DTU_190226_TPS548D21RVFR.pdf
Part Number: TPS548D21 Hello,
I am not clear what is difference if FSEL[2:1] changes. The datasheet says this change internal ramp ratio but I am not sure how to select this.
Mode2 can select external SS and Mode[1:0] can select the ramp time. I am not…
Part Number: TPS548D21 Tool/software: WEBENCH® Design Tools Hello,
I am using TPS548D21 in one of my project and I found in datasheet like Feedback resistors on RSP & RSN should be much lesser than 100K.
But in webench tool when i simulated the schematics…
Part Number: TPS548D21 1. In the PSPICE files provided with TPS548D21, there are two designs, Startup and Steady State, could you tell me what the difference are between two models used in two designs?
2. Could you tell me how to run Bode plot with the…
Other Parts Discussed in Thread: TPS548B22 , TPS548C26 , TPS548D22 , TPS53355 , TPS546D24A , TPS548D21 , TPS54KB20 Hi TI Team, I am looking for a DC-DC Step Down Converter Power Supply IC with Below Spefications. Vin : 11.5V to 12.5V Vin(nom) : 12V Vout : 0.8V Ripple…